2019-06-17 11:38 AM
I have STM32F0DISCOVERY (STM32F051R8Tx). I work on CubeMX and Eclipse. I have a problem with setting EXTI interrupts. Please help.
2019-06-17 11:57 AM
What do you want to do?
Which pin(s) and trigger interrupt on which edge(s)?
Have you set and selected the pin to be "EXTI" on cubemx?
2019-06-18 2:04 AM
PB15 is set: [BAZA] GPIOEXTI15 (no mode). NVIC Enabled EXTI line 4 to 15 interrupts. GPIO mode External Interrupt Mode with Rising edge trigger detection. GPIO Poll-up/Pull-down: No pull-up and no pull-down. User label: BAZA.
I'm generating a program.
I write:
/* USER CODE BEGIN 4 */
void HAL_GPIO_EXIT_Callback(uint16_t GPIO_Pin) {
if (GPIO_Pin == BAZA_Pin) {
HAL_GPIO_WritePin(LED_BAZA_GPIO_Port, LED_BAZA_Pin, GPIO_PIN_RESET);
HAL_Delay(10000);
}
}
after pressing the BASE the LED is not lit.
The LED is well connected because it works when I turn it on and off not interrupt.
2019-06-18 2:10 AM
You should probably avoid delays in the callback.
So if you break-point the IRQ Handler and callback, you catch either in the debugger?
Check pin state.
Review initialization code and handlers.
Review peripheral states/settings/clocks in debugger. ie RCC, SYSCFG, GPIO, etc
2019-06-18 4:28 AM