2024-09-03 2:00 PM - edited 2024-09-03 2:00 PM
I can not download software from Stm32 anymore because I do not receive download links via mail anymore, but I still receive emails for webinar invites.
How could I get the software I need from stm32 now?
2024-09-03 3:13 PM
Welcome @The_Moviemonster, to the community!
I can't remember URLs ever being sent out for downloading STM32 3 software. Just log in on st.com and the download can start. Which software are you interested in?
Regards
/Peter
2024-09-03 3:37 PM
It is a tertiary measure, when you don't want to login, or there's an issue.
Saved a couple of situations where the primary server won't provide from the download page, or was corrupt. Couple of cases with downloads ~1GB as I recall.
2024-09-04 12:10 AM
Ok, I way got confused about the download link. However, I still could not download CubeMX or STM32 Virtual Comport.
Every time I click on download latest I have to accept and log in with my account or use it like a guest. But then nothing happens. (I get redirected to the overview page of the given software, without any download starting)
Not shure why. In the past, I downloaded cubeide with the same account.
Is it possible that the download page gets blocked without me knowing?
(I checked disabling Pihole and also checked the logs, nothing got blocked there.)
2024-09-04 12:13 AM
So does it help that I live in Germany?
Is there a workaround?Not getting the software you need because the download would not start sucks. Also, I did not get any feedback on what went wrong.
2024-09-04 4:35 AM
Hi @The_Moviemonster,
Thanks for reporting this issue.
I'd like you to try logging into your myST account, top right on the front page https://st.com and then start a download.
Let me know if this works.
Best regards,
Laurids