cancel
Showing results for 
Search instead for 
Did you mean: 

How to determine timer clock source on stm32f746

Brother Theo
Associate II

According to MX Cube there are 2 timer clocks, APB1 and APB2. At max APB1 is 108MHz and APB2 is at 216. I can't anywhere where it shows which timer gets which clock.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

It's listed in the register boundary address table. I agree it could be presented better.

Different RM, but probably same information:

0693W00000LyXQqQAN.png 

If you feel a post has answered your question, please click "Accept as Solution".

Usually there's a big bus diagram showing which APB different peripheral live on. I also often dictates which DMA unit will service the peripheral side bus interaction.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

> Usually there's a big bus diagram showing

> which APB different peripheral live on

... at the beginning of every STM32 Datasheet.

JW