cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the output dir for existing CubeMx project?

hmc
Associate III
Posted on July 04, 2016 at 21:55

Hello, is there any way to change the output dir (I guess it's the same as Toolchain Folder Location?) in CubeMX?

#cubemx-output-folder
2 REPLIES 2
Nesrine M_O
Lead II
Posted on July 05, 2016 at 15:53

Hi choi.henry,

I will forward your request to our MX team.

-Syrine-

stm32cube-t
Senior III
Posted on July 19, 2016 at 10:48

Hello,

The project folder can not be changed. The workaround is to save the existing project as a new project: select the menu ''File > Save Project as'' and specify there a new project name (optional) and new destination folder.

Note this will create the project folder and save in there the project .ioc file only.

You will have to click ''generate code'' to retrieve the generated initialization code at the new location.

Best regards