2019-10-16 04:58 AM
2019-10-16 07:25 AM
Hello @Community member ,
Which Cubemx version ?
Try to delete .stm32cubemx folder and tell me is it ok or not.
Best regards,
Khouloud.
2019-10-17 04:24 AM
I have different CubeMX Versions installed (WIN10),
e.g.
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5.2.1
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5.3.0
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5-4-0
Sorry the previous ioc file has a problem with SAI4 BDMA , it does not open with Version 5.3.0 or 5.4.0.
I have mentioned this in another post. Please check also this problem.
see attached log file
...
2019-10-17 11:19:52,071 [FATAL] ProjectFactory:336 - Exception caught
java.lang.NullPointerException
...
--------------
to delete .stm32cubemx in windows users directory is not the best idea, I loose the settings in Cubemx package manager, no more firmware is installed.
I have renamed .stm32cubemx and could revert back to original settings.
--------------
I have attached another .ioc file which was created with MxCube.Version=5.2.1
For test I have copied only the .ioc file in another folder (nothing else in this folder).
It seems that there are some settings which change if I open this file with different CubeMX versions.
try to open with 5.4.0
--> wrong message that FW_H7 V1.4.0 is not available in repository (but FW_H7 V1.4.0 is installed)
I press cancel !
try to open with 5.3.0
--> correct message that FW_H7 V1.4.0 is not the latest
I press cancel !
try again to open with 5.4.0 (double click on .ioc file)
--> project opens normal with no migration dialog
I press cancel !
try again to open with 5.4.0 (double click on .ioc file)
--> wrong message that FW_H7 V1.4.0 is not available in repository
I press cancel !
that's really confusing ?
2019-10-17 06:17 AM
Hello @Community member ,
Thanks for your feedback, It will be internally checked.
Best Regards,
Khouloud