cancel
Showing results for 
Search instead for 
Did you mean: 

Hi! I am trying to install the STM32CubeMX 6.8.0 on my macOS 13.3 (Ventura),when I run the installer it gives me the following error: You cannot open the application SetupSTM32CubeMX-6.8.0.app because it is corrupted or incomplete.

CColo.2
Associate II

I have installed Xcode and tried to run the instructions "In case of error, try one of the following fixes: - $sudo xattr -cr ~/SetupSTM32CubeMX-6.8.0.app."

2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @CColo.2​ 

First let me thank you for posting .

Let's try to uninstall and reinstall CubeMX again .

This is the LINK to download the Latest version CubeMX 6.8.0

Uninstalling STM32CubeMX on macOS® :

There are two different ways to uninstall STM32CubeMX on Mac:

1. Move STM32CubeMX.VERSION.app to the trash

2. Use the following command line:

a) For STM32CubeMX 6.2.x and later versions only: cd SetupSTM32CubeMX-VERSION.app/Contents/Resources/Uninstaller ./uninstall.s

To install CubeMX 6.8.0 On macOS please follow those steps :

a) On STM32CubeMX-Mac line, Click “Get software�? to download the package 

b) Extract (unzip) the downloaded package.

c) Make sure you have administrator rights. 

d) Double-click SetupSTM32CubeMX-VERSION.app application file to launch the 

installation wizard.

In case of error, try to fix it: - $sudo xattr -cr <Folder where the zip was extracted>

Thx

Ghofrane

CColo.2
Associate II

Hello Ghofrane GSOURI,

Thank you, the problem I had was the Beta version of macOs Ventura 13.3, it wouldn't let me install the software, I reinstalled the normal Ventura 13.3 version, I installed the CubeMX 6.8.0 version without a problem and then I updated to the Beta version of the macOS.