2016-09-08 7:57 AM
Hello,
I am trying to send 1000 values from data stored in DMA on to CAN Bus. i am using the Data frame(8 bits each) of CAN to transmit data but i am not able to receive all the data frames. i am not able to understand what is the problem . i am using HAL Library and STM32F4_Discovery board. Have attached the CAN related code. uint16_t IT_buffer[1000]; // buffer storing 1000 values/*CAN Transmit*/void CAN_Tx(void){volatile int j=0;volatile int b=0; for(j=0;j<250;j++) // each time 4values out of 1000values are send therefore 1000/4=250 { //♯♯-3- Start the Transmission process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯ CanHandle.pTxMsg->StdId = 0x123; CanHandle.pTxMsg->RTR = CAN_RTR_DATA; CanHandle.pTxMsg->IDE = CAN_ID_STD; CanHandle.pTxMsg->DLC = 8; CanHandle.pTxMsg->Data[0] = (IT_buffer[b] >> 8); CanHandle.pTxMsg->Data[1] = (IT_buffer[b]); CanHandle.pTxMsg->Data[2] = (IT_buffer[b+1] >> 8); CanHandle.pTxMsg->Data[3] = (IT_buffer[b+1]); CanHandle.pTxMsg->Data[4] = (IT_buffer[b+2] >> 8); CanHandle.pTxMsg->Data[5] = (IT_buffer[b+2]); CanHandle.pTxMsg->Data[6] = (IT_buffer[b+3] >> 8); CanHandle.pTxMsg->Data[7] = (IT_buffer[b+3]); TransmitMailbox = HAL_CAN_Transmit(&CanHandle, 30); b=b+4; }}/* CAN1 init function */void MX_CAN1_Init(void){ HAL_CAN_DeInit(&CanHandle); static CanTxMsgTypeDef TxMessage; static CanRxMsgTypeDef RxMessage; /*♯♯-1- Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ /*Baurd rate defined at 1Mhz */ CanHandle.Instance = CAN1; CanHandle.pTxMsg = &TxMessage; CanHandle.pRxMsg = &RxMessage; CanHandle.Init.TTCM = DISABLE; CanHandle.Init.ABOM = DISABLE; CanHandle.Init.AWUM = DISABLE; CanHandle.Init.NART = DISABLE; CanHandle.Init.RFLM = DISABLE; CanHandle.Init.TXFP = DISABLE; CanHandle.Init.Mode = CAN_MODE_NORMAL; /* CAN Baudrate = 175kbps (CAN clocked at 42 MHz) */ CanHandle.Init.SJW = CAN_SJW_1TQ; CanHandle.Init.BS1 = CAN_BS1_6TQ; CanHandle.Init.BS2 = CAN_BS2_8TQ; CanHandle.Init.Prescaler = 16; HAL_CAN_Init(&CanHandle);}/*CAN1 filter function*/void CAN_filter_init(void){ CAN_FilterConfTypeDef sFilterConfig; /*♯♯-2- Configure the CAN Filter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000;//0x100 << 5;; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000;//0x700 << 5; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = CAN_FILTER_FIFO0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber =14; HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig);}can any one help me please!!! #stm32 #hal #can #cubemx #canbus2016-09-09 4:48 AM
the only thing 175kbits are very uncommon for a can-bus (at least in the automotive)
100 - 125- 250 - 500 if everything is ok with your baudrate and samplepointer @ 75-85% check your network bus-termination 60ohms for a highspeed network between can-high and can-low2016-09-09 6:45 AM
Hi saraf.ninad.001,
Which pins you are using (TX/RX). How you have configured the GPIOs ? Share also your main() function to see how you manage your application and how Transmit/receive functions are called. -Hannibal-