FLASH.ld syntax error when upgrading to CubeMX v6.12.1
- 2 replies
- 4184 views
Hello,
Since the latest release of CubeMX (6.12.1) installed, I have been encountering syntax errors related to the "FLASH.ld" file.
This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32F103C8T6.
It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.
I have also included the FLASH.ld file that was generated for your reference.
The terminal output the wrong as below , after run the default cmake-build task with the project templete generated by CubeMX (6.12.1) :
STM32F103C8Tx_FLASH.ld:56: syntax error
collect2.exe: error: ld returned 1 exit status
ninja: build stopped: subcommand failed.
build finished with error(s).
Then, after replacing 6.12.1 flash.ld with 6.12.0 flash.ld , the errors are eliminated.
Here are two versions of the flash.ld attached.
---
Thanks for your help.