cancel
Showing results for 
Search instead for 
Did you mean: 

Error setting up dual bank quad SPI

When I try to set up quad SPI with dual bank on an STM32H7, I get the following message:

"You must select a ChipSelect signal for Dual bank mode first"

This is true even for a blank project with nothing else assigned. I don't see anywhere available to select the chip select lines.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud ZEMMELI
ST Employee

​Hello @Adrian Adamson​ 

Thanks for the feedback.

You are right, This issue will be fixed in the next CubeMX release.

Best Regards,

Khouloud.

View solution in original post

3 REPLIES 3
Khouloud ZEMMELI
ST Employee

​Hello @Adrian Adamson​ 

Thanks for the feedback.

You are right, This issue will be fixed in the next CubeMX release.

Best Regards,

Khouloud.

Thank you for your help. Hopefully the update will be soon. I'm working on the board layout now and I do need to know which pins to route to for those chip selects. I guess for now I should assume that they are the same pins used for NSS in the other QSPI modes?

Will PM you schematic section I've worked from.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..