cancel
Showing results for 
Search instead for 
Did you mean: 

Error Log: CubeMX plugin appears to be active, Log4j initialization might be too late.

BHime
Associate II

I am running STM32CubeIDE Version: 1.11.2 Build: 14494_20230119_0724 (UTC). When I startup CubeIDE, I am seeing the following error in the Error Log: 

"CubeMX plugin appears to be active, Log4j initialization might be too late."

I would appreciate it if someone could point me in the correct direction to resolve it (or ignore it). I am relatively new to CubeIDE, as I have primarily been doing my STM32 work from the command line with Makefiles. CubeIDE seems to be working fine so the error is not slowing me down at the moment.

10 REPLIES 10
Moza
Associate II

I also have the same error.

CubeMX plugin appears to be active, Log4j initialization might be too late.

eclipse.buildId=Version 1.15.1
java.version=17.0.8.1
java.vendor=Eclipse Adoptium
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Command-line arguments: -os linux -ws gtk -arch x86_64