cancel
Showing results for 
Search instead for 
Did you mean: 

Error in adc.c generated by STM32Cube FW_G4 V1.5.2

Yves Bmnt
Associate III

Hi all,

just found an error preventing the adc from working properly when the driver is generated by STM32Cube FW_G4 V1.5.2 (and 1.5.1).

there are some missing lines like this one:

sConfig.Channel = ADC_CHANNEL_2;

 

you can compare my 2 attached files to see for yourself.

kind regards,

Yves

 

1 ACCEPTED SOLUTION

Accepted Solutions
Souhaib MAZHOUD
ST Employee

Unfortunately, I was unable to reproduce the problem with FW_G4 V1.5.2.
Could you please ensure that you have changed the channel name under Rank as bellow:

 

SouhaibMAZHOUD_0-1709827219776.png

 

 

 

View solution in original post

4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @Yves Bmnt 

Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.

Thx

Souhaib

Yves Bmnt
Associate III

Maybe it can help, I had the ok file generated by STM32CubeMX V6.61 (using STM32Cube FW_G4 V1.5.1), and the ko file generated by STM32CubeMX V6.9.2 (using STM32Cube FW_G4 V1.5.2) so it probably doesn't come from the STM32Cube FW_G4, unlike mentioned in my previous post.

Yves

Souhaib MAZHOUD
ST Employee

Unfortunately, I was unable to reproduce the problem with FW_G4 V1.5.2.
Could you please ensure that you have changed the channel name under Rank as bellow:

 

SouhaibMAZHOUD_0-1709827219776.png

 

 

 

Yves Bmnt
Associate III

Thank you so much, I missed that when migrating the microcontroller!

Yves