cancel
Showing results for 
Search instead for 
Did you mean: 

does not support the system thread viewer on cubemx with keil v5.x ?

Fish
Associate II

hi,

i have questions about cubemx with stm32f series

i'm testing the stm32f with cubemx + keil v5.26

originally, i have created many projects using keil CMSIS Pack Installer with classic methode

in this project, i can debug thread list on real time when i entered the debug mode

but, after i have created a project using CubeMx with keil, i can't see the thread list and status

image here..

case 1: can see the thread list and status

0693W00000QN7aVQAT.jpg 

case 2: can't see the any information

 0693W00000QN7aaQAD.jpgdoes anyone know this?

thank you in advance

2 REPLIES 2

Not sure anyone's going to chase down issues in older versions of Keil. Current is 5.37

In more recent times I've had to pull packs via the Cube HAL directories.

If it's still broken perhaps push in as an Online Support request, but a lot of the EU side teams are out for August.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

thanks :loudly_crying_face: