cancel
Showing results for 
Search instead for 
Did you mean: 

Does CubeMX can be utilized to develop applications for CortexA processors? in this case, which is the OS supported? is there any RTOS supported? Cube MX can also be utilized to program Cortex R (Accordo 2) product?

Hicss.2033
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Hello Hicss.2033,

STM32CubeMx covers the whole portfolio of STM32 microcontrollers, based on 32-bit Arm Cortex cores. It allows configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization C code for the Arm® Cortex®-M core or a partial Linux® Device Tree for Arm® Cortex®-A core.

It is available as standalone software running on Windows®, Linux® and macOS® (macOS is a trademark of Apple Inc. registered in the U.S. and other countries.) operating systems, or through Eclipse plug-in.

For more details check: https://www.st.com/en/development-tools/stm32cubemx.html.

FreeRTOS™ is the class of RTOS is used to run on STM32 microcontroller or microprocessor. For more details please refer to the UM of Developing applications on STM32Cube with RTOS: https://www.st.com/resource/en/user_manual/dm00105262-developing-applications-on-stm32cube-with-rtos-stmicroelectronics.pdf

Best Regards,

Khouloud.