2025-01-23 2:04 AM - last edited on 2025-01-23 3:02 AM by mƎALLEm
Why can't I change the Firmware Relative Path when I have unchecked the "Use Default Firmware Location"?I clicked the "Browse" button and there was no response.
2025-01-23 2:06 AM
And the "Browse" button of project lacation.
2025-01-23 3:04 AM
Hello,
Need to show more, especially when you click on Browse button. Show a screen shot when you click on browse button.
+ provide what CubeMx version you are using.
2025-01-23 3:22 AM
Thank you for your reply. The screenshot I uploaded is the screenshot after I clicked the browse button, which means that the screen has not changed when I clicked the browse button. I used the latest version downloaded by official website.
2025-01-23 3:50 AM
I didn't reproduce the issue with the latest version of CubeMx 6.13.0.
Did you find it as a regression? I mean it worked previously then the issue occurred?
2025-01-23 4:00 AM
I just downloaded it and haven't used it before.
2025-01-23 4:00 AM
Related: https://community.st.com/t5/stm32cubemx-mcus/browse-button-on-cubemx-not-working/td-p/764102 ?
Do none of the 'Browse' buttons anywhere in your CubeMX work?
2025-01-23 4:11 AM
Yes!This bothers me very much.