cancel
Showing results for 
Search instead for 
Did you mean: 

[CubeMX regression]Failed to generate code with 4.22.1

martonmiklos
Senior
Posted on September 13, 2017 at 08:46

The new CubeMX 4.22.1 fails to generate code (and hangs on generation) for a STM32 workbench project which has been successfully generated with the previous versions.

Here is the command line output from the problem:

https://pastebin.com/kgumCq6t

 

I am using Linux please see the ioc file attached. The error also occurs when generating blank project.

#bug #regression #cubemx-4.22
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
martonmiklos
Senior
Posted on September 15, 2017 at 13:12

This issue only happened with an updated 4.22.1 CubeMX. After reinstallation it works fine.

View solution in original post

1 REPLY 1
martonmiklos
Senior
Posted on September 15, 2017 at 13:12

This issue only happened with an updated 4.22.1 CubeMX. After reinstallation it works fine.