2018-05-23 03:53 AM
Hello guy.
I' upgrade my CubeMX software to V.4.25.1 every thing is clear no problem. But when we try to generate MDK project CubeMX show an project generate problem ( see in attach pic.)
Please tellme how to fix it
Thank you
EDIT!!:: TrueStudio has the same problem.
#cubemx-4.25 #mdk-arm2020-04-14 12:50 AM
Thanks. it works for me. My problem is that I have installed jdk14 for some java development. I uninstall jdk14 and install jdk8, now it's OK.
2020-05-07 01:17 AM
Шановний, що �?аме, коли у мене така ж проблема? Я прочитав �?вої відповіді та згадав, що �?творив нову машину java. Що �?то�?уєть�?�? проблеми, що конфліктує між Куб - Java -
2020-06-01 06:45 AM
У мен�? така�? же проблема! �?е получает�?�? �?генерировать проект, под keil 5...�?ичего из вышеперечи�?ленного не помогает, �? бы не хотел переу�?танавливать windows из-за одной программы... Please help me...
2020-06-01 12:15 PM
Everything is fine and working with
java version "1.8.0_191"
Java(TM) SE Runtime Environment (build 1.8.0_191-b12)
2020-06-18 03:26 AM
Is there a solution to this problem?
2020-06-19 07:18 AM
I have the same problem. The problem is related with Java Run Time Enviroment Version, i back to 8.231 version and works fine.
2020-07-23 12:35 AM
If you still have this issue in version 5.6.1 try to install OpenJDK instead of Java(SE)
FIX: Downloaded the OpenJDK from here:
2020-08-04 06:42 AM
Today I noticed this problem too (CubeMX version 6.0.0). I was sure that the problem was in Java and was not mistaken. I reinstalled Java several times using the installer downloaded from the Java.com website but did not help. Then I downloaded the full installation (offline version), reinstalled it and the problem was solved.
2020-08-07 12:54 AM
i'm facing this problem after updating to ver 6.0.0. I tried reinstalling it on other folder location
but the problem was not solved. need to fix as the projproject is stuck.
2020-08-29 05:58 AM
Hello All,
I faced the same issue and I solved my problem on my own.
You guys might be facing the issue due to same reason.
Please Follow these steps.
4. After matching the java version, please restart the PC(This is important).
5 Still doesn't work ? Uninstall completely including program data and settings and follow the above steps.
Kind Regards
Sandeep Saxena