cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMx issue: fixed FDCAN Tx buffer allocation = 32

MHoll.2
Senior III

Split from this thread.

Yes, but No!
CubeMX V6.16 now allows only exactly 32 TX Buffers ((TX Buffer Nbr + TX Fifo Queue Elmts Nbr) == 32).
But less then 32 TX Buffer is allows by the Hardware, and some times, required if You want to maximize the RX Buffers.

1 ACCEPTED SOLUTION

Accepted Solutions
Ghofrane GSOURI
ST Employee

Hello @MHoll.2 

The CubeMX should allow (TX Buffers Nbr + TX FIFO Queue Elmts Nbr ≤ 32 ) instead of ((TX Buffer Nbr + TX Fifo Queue Elmts Nbr) == 32

A ticket (ID: 222211) has been escalated to the development team to address and correct this behavior.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @MHoll.2 

The CubeMX should allow (TX Buffers Nbr + TX FIFO Queue Elmts Nbr ≤ 32 ) instead of ((TX Buffer Nbr + TX Fifo Queue Elmts Nbr) == 32

A ticket (ID: 222211) has been escalated to the development team to address and correct this behavior.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @MHoll.2 

This issue has been resolved in the latest version of STM32CubeMX 6.17.0 

Link to download 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.