CubeMX ignores some settings in .ioc file
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-01 9:14 AM
There appears to be a bug in STM32CubeMX where some settings are not loaded when reopening the app and project, even though they were previously successfully written to the .ioc file. Default settings are always used instead, and then re-saving the project (without making any changes yourself) will write these undesired settings back to the .ioc file. These settings are:
- Project Manager > Project > Firmware Location (custom path reset back to default path)
- Project Manager > Project > Add library files as reference (reset back to copy)
Steps to reproduce:
- Create a symlink to `STM32Cube/Repository` which is relative to the intended project workspace. This enables sharing projects among multiple developers, since CubeMX uses a relative path to the FW repo.
ln -s ~/STM32Cube/Repository ~/projects/demo/cube_repo
- Launch CubeMX, and create a new project with the following settings:
- Save and close CubeMX. This produces a .ioc file.
- Track the .ioc file with version control (this gives us more info about the upcoming bug).
- Reopen CubeMX and the previous project, note that the following settings have been reset:
- Save the project. This updates the .ioc file, even though we did not intend to make any changes. Here is the `git diff` output showing what was reset in the .ioc file:
-ProjectManager.CustomerFirmwarePackage=../../cube_repo/STM32Cube_FW_F4_V1.25.0
+ProjectManager.CustomerFirmwarePackage=../../../../STM32Cube/Repository
-ProjectManager.LibraryCopy=2
+ProjectManager.LibraryCopy=1
System info:
- OS : Ubuntu 20.04
- STM32CubeMX version: 6.0.1
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-14 6:02 AM
Hello @Miles​ ,
Thanks for bringing this to our attention, Issues confirmed an they will be fixed.
Best Regards,
Khouloud
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-03 6:19 PM
This is also an issue when running STM32CubeMX in command line mode.
For example with this script (saved as mxcmd.txt):
config load /home/miles/projects/demo/cube_workspace/test1/test1.ioc
project generate
exit
And executed with:
/home/miles/STM32CubeMX/STM32CubeMX -q $(readlink -f mxcmd.txt)
It overwrites the .ioc file with the same changes as described in the previous message, and then generates project output with these undesired settings.
Two other annoyances with the CLI interface:
- It launches a splash screen. This shouldn't happen for a CLI app. I'm concerned this will cause issues when running in a headless environment.
- It requires an absolute path to the script. I'm using readlink as a workaround.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-14 6:02 AM
Hello @Miles​ ,
Thanks for bringing this to our attention, Issues confirmed an they will be fixed.
Best Regards,
Khouloud