cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX: How to set generated IAR project name ?

AndreaTW
Associate II

Hi,
I'm using CubeMX 6.16.0 with the EWARM setting.
When I click "Generate Code," it creates the IAR project with the default name "project.eww."
I open the project with IAR and save it with a new name.
Then I click the "Generate Code" button on CubeMX, and it regenerates the workspace name, again as "project.eww."

Is it possible to set the IAR project name from CubeMX to something other than "project.eww"?

Thanks

5 REPLIES 5
TDK
Super User

Not directly. You could rename it via a post-code generation script.

If you feel a post has answered your question, please click "Accept as Solution".
Chris21
Senior III

It does seem odd that the Project Name is not used for the workspace file.  

You could ignore the project.eww and use your new named workspace file, nothing will change in project.eww.

If I save the IAR project with another name (e.g. prova.eww), when I use CubeMX to "Generate code" it deletes the project "prova.eww" with "project.eww".

Good idea but a bit complicated, not easy to manage among work colleagues

-> it deletes the project "prova.eww"

CubeMX generated a new "project.eww" but did not delete the eww file that I renamed.