2015-05-03 10:53 AM
Hello, I have an olimex E407 board featuring stm32f407zgt. I create a simple application using cubeMX and want to ping.
The board receives packets (I can see this using LWIP_DEBUG functionality) but the TX does not work. In xxx_hal_eth.c in the function HAL_ETH_TransmitFrame: Tx DMA seems blocked and the code runs into this section: /* When Tx Buffer unavailable flag is set: clear it and resume transmission */ if (((heth->Instance)->DMASR & ETH_DMASR_TBUS) != (uint32_t)RESET) { /* Clear TBUS ETHERNET DMA flag */ (heth->Instance)->DMASR = ETH_DMASR_TBUS; /* Resume DMA transmission*/ (heth->Instance)->DMATPDR = 0; } I do not see any ETH frame being transmitted. Any hints? Regards, Adib. -- #cubemx #stm32f4 #ethernet2015-05-15 4:34 AM
I found that once after a coldboot it works.
So poweroff/poweronn: ok. reset: not ok. Adib.