2018-01-07 4:14 PM
Suppose that a hardware developer wants to pass in a Cube file some info for a fellow programmer.
For example tell which UART or GPIO pin to use:
&sharpdefine RS232_UART USART4
&sharpdefine LED_PIN (GPIOB, 10)
But Cube won't allow this. It understands only literal numbers and quoted strings.
It will allow
&sharpdefine RS232
_UART 'USART4' - but this is completely useless for the purpose.
How hard would be enabling any user definition text in the Cube code generator?
Regards,
- pa
#cube-mx2018-01-07 9:56 PM
Any pin definition can be set in the graphical view of the microcontroller and is included in the main.h when the code is generated. When I do my own libraries, I decide a standard for naming the pins used in my library, a standard that any user that use my library must follow (of course, I include a comment that describe this obligation in my library's header)
As for any other 'parameters', I do defines before including the headers of my libraries (and mentioned in the library documentation). By example, a device that use I2C, in the main.c file I indicate which I2C peripheral the device should use via a #define before include:
#include <main.h>
#define device_x_use_I2C1
#include 'device_x_library_header.h'
�?�?�?�?�?�?
Inside the 'device_x_library_header.h' file I do:
#ifdef device_x_use_I2C1
//use the I2C1 parameter in your I2C functions
#else
//use the I2C2 parameter in your I2C functions
#endif�?�?�?�?�?
I use CubeMX for generating the required initialization code but I use my own 'repository of libraries' built upon LL drivers. I find the pin naming mechanism in the CubeMX to be enough in providing user standardized libraries, without adding something inside CubeMX.
What I would like to have in the 'Project settings' window is a possibility to define a relative path to my (user) repository of libraries/headers.
2018-01-08 4:07 AM
Hi Vasile,
Of course ifone has a .h filehe can put anything there. Butmy hardware developers use only the cube to select pins, map pins to on-chip devices, set GPIO pin modes and so on. From them I receive only .ioc files.
#define device_x_use_I2C1
is good enough though. Thank you.
-- pa
2018-01-08 7:06 AM
#define LED_PIN (GPIOB, 10)
But how would you actually use that in your code?
2018-01-08 8:38 AM
Neil.Andrew
- This will require some macro on the programmer's side, like, er....#define MY_GPIO_INIT(g,p) { .m_gpio = g, .m_pin = p }
struct { GPIO_typedef *m_gpio, uint16_t m_pin } my_pin = MY_GPIO_INIT(LED_PIN);
We just need some simple conventionwith the h/w guy, easy to understand and remember
By the way,he canspecify the active pin state too:
#define LED_PIN (GPIOB, 10, 1)
...
#define MY_GPIO_INIT(g, p, s) { .m_gpio = g, .m_pin = p, m_on_state = s }
struct { GPIO_typedef *m_gpio, uint16_t m_pin,bool m_on_state } my_pin = MY_GPIO_INIT(LED_PIN);
-- pa
2018-01-08 8:44 AM
pavel a wrote:
This will require some macro on the programmer's side,
Exactly - that's all outside the scope of CubeMX.
I guess you could make a utility that parses the CubeMX output to create this sort of thing ...
2018-01-08 8:59 AM
But I don't ask that Cube provides these macros or use them in generated code.
I'm only asking to let me specify any text as the macro value, and put it into the .ioc file as is.
Other person who will generate code from this .ioc will deal with it.
It is for situations when the h/w guy decides to change a pin or its level, makes a quick fix in the cube and sends the .ioc file back to s/w dev. The latter (me) will re-generate code from the .ioc, and it will work automagically.
Sure, the programmer can write a quick python script to fetch and convert certain quoted strings from the .ioc file and add a custom build step in the toolchain. But the poor h/w guy will have to add quotes around some of definitions but not others.... Not elegant :(
-- pa
2018-01-08 9:08 AM
Forgot to ask: are the 'user constants' just a passive payload for code generation, or the Cube interprets /uses them for something? After editing a definition, it writes 'replacing the value in all occurrences' or smth like this.
-- pa