cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX configuration not possible for my board and LCD expansion?

ChrisCanelea
Associate

Hello,

I am currently trying to program a NUCLEO-F446ZE with an X-NUCLEO-GFX02Z1 display expansion board. From the data brief, I have confirmed the compatibility of the display with my specific board, however, when attempting to use CubeMX with X-CUBE-DISPLAY to configure it, I have run into a dead end and cannot seem to configure it at all. Upon looking at the X-CUBE-DISPLAY documentation in the STM32Cube repository, I find that the NUCLEO-F4xx is not on the list of supported boards. Is there simply no way for me to use CubeMX to configure the display with my board? If this is the case, can anyone point me in the right direction on where to start?

Any help is appreciated in this matter, attached below is the data brief list showing my board, followed by the documentation list of supported boards.

ChrisCanelea_0-1710905917886.png

ChrisCanelea_2-1710906254459.png

 

 

 

0 REPLIES 0