2015-03-02 3:30 PM
Hi,
I did a initialization project with CubeMX for STM32F4discovery but when I click ''generate source code'' (selecting IDE MDK-ARM 4.73 and firmware package STM32Cube FW_F4 V1.4.0) appears the error message:''the code is succesfully generated under [.....] but MDK-ARM 4.73 generation project but have a problem''.How can I fix the error?Thank you so muchNF #stm32f4 #discovery #cubemx2015-03-05 1:50 AM
Please ensure the product Pack is installed with your toolchain. You may check out the following link for the install procedure: [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Problem%20with%20CubeMX%204.5.0&]Link
2015-03-18 11:56 AM
Could bit detail explain how to fix it? Because I have same exactly same problem. I used KEIL and it works perfect. I install STM32Cube and it can not generate project file, so for my mind problem is in STM32Cube or in the way how I install it.
2015-03-20 3:33 AM
2015-11-17 6:23 AM
Hi,
I do have the same error. I am working on Windows 10 and using STM32CubeMX 4.1.11.0 and Keil uVision V5.17.0.0. I want to program a STM32F429I discovery board. When I generate the project, I get the same error. All device packs are installed. Is there somewhere some more information about the error. ''... but MDK V5 have a problem.'' is not enough information to solve the issue.Thanks in advance for your help.2015-11-21 3:54 AM
Hi,
my problem was a letter of my name. I had installed CubeMX in path with a special character (ò). Installing the software in another path I have solved the problem.ByNifed