2018-11-06 12:28 AM
Hi,
Since cubeMX 4.27, in the function of MX_RTC_Init()
there are no more /* USER CODE BEGIN RTC_Init X */ to add code.
We need this to add test is there is an external battery to save the calendar.
Regards,
Sébastien
2018-11-06 02:06 AM
Hi @COSEBE ,
We will check this and answer you ASAP.
Khouloud.
2018-11-13 12:40 AM
Hello @COSEBE ,
Thanks for your feedback.
Unfortunately I'm not able to reproduce your issue, in MX_RTC_Init with 4.27.0 there is two user code :
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
Could you please give more details (MCU, RTC configuration,..) or may be send me your ioc if possible?
Regards,
Houda
2018-11-13 12:50 AM
2018-11-13 12:58 AM
no attached file can you send again?
2018-11-13 01:02 AM
2018-11-15 04:56 AM
Sorry @COSEBE but not yet received :smiling_face_with_smiling_eyes:
2018-11-15 05:45 AM