cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.13.0 and MCU Package H7 v1.12.0 produce incorrect PCLK frequencies

djanovy
Associate III

I updated to CubeMX 6.13.0 and firmware package 1.12.0 for and STM32H755BIT chip and found several issues with the new release:

  1. Where is it documented that the new ExitRun0Mode() requires 'USE_PWR_LDO_SUPPLY" to be defined if I want to use that mode?  Shouldn't it be defined by CubeMX when the power parameters are selected in the RCC section?
  2. If I am using the Voltage regulator in the LDO supply mode (see RM0399, p 274, Fig. 22, Section 1), what is the purpose of defining SMPS in line 217 of stm32h755xx.h?  In line 440 of system_stm32h7xx_dualcore_boot_cm4_cm7.c the define of SMPS is used to disable the SMPS - shouldn't the define be used to enable the SMPS?
  3. Worst issue:  The clock rates returned from PCLK function calls shown below are now showing 240 MHz!  This has messed up the USARTs and all the timers. I thought the MAX clock rate for the PCLK clocks were 120 MHz (see DS12919, p. 110, Table 23, fPCLK, at VOS0 setting).

 

HAL_RCC_GetPCLK1Freq();
HAL_RCC_GetPCLK2Freq();

 

Screen capture showing 240 MHz clock rate on PCLK:

djanovy_0-1733156463235.png

 

20 REPLIES 20

It is defining both USE_PWR_LDO_SUPPLY and USE_PWR_DIRECT_SMPS_SUPPLY  in the generated CMake file.  It should only define USE_PWR_DIRECT_SMPS_SUPPLY since that's the selected power mode in CubeMX.  I believe this is just a bug with STM32CubeMX code generation.

If I bump your SYSCLK to 280 MHz (max value) the generated CMakeList.txt file only contains:

target_compile_definitions(stm32cubemx INTERFACE 
	USE_PWR_DIRECT_SMPS_SUPPLY 
	USE_HAL_DRIVER 
	STM32H7B3xxQ
    $<$<CONFIG:Debug>:DEBUG>
)

It is confusing how and what the different options are.

cvanbeek
Associate III

That's very interesting.  On my original project I ran into this issue, I have the clock set to 280 MHz.  I can't share that IOC file unfortunately, but it seems like there's a bunch of things happening in the background that may effect this issue.

The requirement for the new defines are discussed in the Main Changes section of the Release Notes for H7 Firmware:

Release Notes for STM32CubeH7 Firmware on Github 

@Ghofrane GSOURI is ST aware of the issue I mentioned (CubeMX creating multiple different USE_PWR* definitions) so that it may be fixed in a future version of STM32CubeMX?

Hello @cvanbeek 

I Couldn't reproduce the issue with a new project starting from scratch but a ticket has been raised to dev team for further investigation to identify the root cause of this behavior (internal ticket number 197797 )

THX

Ghofrane

Hi @Ghofrane GSOURI,

Thank you for noting the issue.  Here's more info on my environment and the example I generated with this issue.

Environment:

  • Windows (we've reproduced this on Windows 10 and Windows 11)
  • STM32CubeMx version 6.13.0
  • STM32Cube FW_H7 V1.12.0

Steps to generate a project with the error:

  • Create a new project for STM32H7B3LIH6Q in CubeMX
  • Select 'No' when asked about configuring MPU
  • Give the project a name
  • Change the toolchain/IDE to 'CMake'
  • The RCC tab already has the supply set to PWR_DIRECT_SMPS_SUPPLY, so no change is needed there
  • Click 'Generate Code'

The resulting cmake/stm32cubemx/CMakeList.txt file has the incorrect USE_PWR_LDO_SUPPLY definition:

cvanbeek_0-1733412996751.png

djanovy
Associate III

I see ST updated the FW_H7_1.12.1 package:

STM32CubeH7 Firmware Package V1.12.1 / 06-December-2024

Main Changes

  • General updates to fix known defects and enhancements implementation.
  • Fix wrong computed clock frequencies in HAL RCC driver.

I'll try it out and see if it fixed the clock issue I was having.

Edit: tagging @Ghofrane GSOURI 

peterdonchev
Senior

After upgrading to CubeMX 6.13.0 and FW_H7_v.1.12.1, I got the following error: undefined reference to `ExitRun0Mode'.

system_stm32h7xx_dualcore_boot_cm4_cm7.c was not regenerated at all. I need to delete it to trigger the generation of a new system_stm32h7xx_dualcore_boot_cm4_cm7.c

 

 

 
 

Same here. When regenerating with CubeMX 6.13.0, some functions disappear. These were present on the first generation of code. Re-generating deletes them and build fails. However, this is not always the case. Sometimes re-generation does work. Not sure how to reliably repeat this.

If it fails, what is missing is `ExitRun0Mode'