2024-12-02 8:49 AM
I updated to CubeMX 6.13.0 and firmware package 1.12.0 for and STM32H755BIT chip and found several issues with the new release:
HAL_RCC_GetPCLK1Freq();
HAL_RCC_GetPCLK2Freq();
Screen capture showing 240 MHz clock rate on PCLK:
2024-12-30 7:08 PM
Hi, @djanovy
I ran into same issue as you
1. RCC clock generation is wrong.
2. Both USE_PWR_LDO_SUPPLY and USE_PWR_DIRECT_SMPS_SUPPLY are defined.
Not understand why ST has sucu low level issue. After you tried out FW_H7_1.12.1, are these issue resolved?
Peter
2025-07-11 10:27 AM - edited 2025-07-11 10:40 AM
Did you ever find a solution to this? I'm trying to build a TouchGFX sample for a Riverdi board, and I am getting:
undefined reference to `ExitRun0Mode'and, as was noted above, the system_stm32h7xx_dualcore_boot_cm4_cm7.c file is only regenerated if I delete the original one.
I am using FW_H7_1.12.1.
Edited to add:
ExitRun0Mode is defined in (the regenerated) system_stm32h7xx_dualcore_boot_cm4_cm7.c, so it looks like it may not be getting pulled into the build (using cmake).
2025-09-05 3:00 AM
My solution was to take a detour and using the Before/After scripting offered by CubeMX. In Project Manager/Code Generator you can find user actions section with before and after code generation commands.
I made suitable scripts to preserve my original code and then restore it after cubemx finishes. This works nicely for things that you need to preserve.