2018-10-09 5:49 PM
My reading of the specs for the F7 series is that if an external clock is supplied to RCC_OSC_IN and HSE Bypass mode is selected then RCC_OSC_OUT is available as a general GPIO pin.
CubeMX seems to want to assign it so I loose a pin!!
2018-10-09 5:57 PM
Never mind - read the wrong paragraph...
2018-10-09 7:56 PM
Should generally be usable, but might behave oddly with code that doesn't understand/use BYPASS, perhaps the System Loader?
I have concerns with L0 parts, a 32 MHz input clock does not permit BYPASS mode, where as an 8 MHz one works as expected.