cancel
Showing results for 
Search instead for 
Did you mean: 

Configuring USART3 error while deploying deep learning model in NUCLEO-H753ZI

I installed stm32CubeIDE version 1.18.0
Started a new stm32 project, selected my board, clicked ok for everything (like it showed a window which contained 5 checked options of led,virtual port etc etc.), i selected all and clicked ok.
Then activated XCubeAI package, checked core and selected validation under application, then clicked on OK.
Then i tried to open that network window... but before that a small window opened which showed configuring usart3 and it got stuck at 70% for very long time... i tried closing the app and disconnecting, restarting pc... but the same thing is happening... i shared a screenshot of where it got stuck...
PLease help me with this...

Pinagadi_Meghana_0-1741602563524.png

 

 

26 REPLIES 26

C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+dp/hard\libc_nano.a(libc_a-signalr.o): note: the message above does not take linker garbage collection into account

see i am getting this error... how many times ever i tried to build
please help me through this

Please respond to my error message.... Help me with that single error. . My work will be done.

 

note: the message above does not take linker garbage collection into account

Which message above? What exactly is the error? If these are only warnings and the executable file is created - ignore these messages. All of them.

 

Sir... Please respond

Pinagadi_Meghana_0-1741833182714.png

 

See... It has one error and one warning... I thought the red coloured one is error and i copied that one...
if the yellow one is the error... 
It is preventing the build...
PLease tell me the solution...
i tried implementing kill in syscalls.c under core>src multiple times...
But how many ever times i did that and saved... after i click clean and build... it is showing that error and when i recheck the file... syscalls.c file which i created earlier is present anymore there... I tried and failed multiple times....
What is the problem????
(BTW i dont use any kill function...)

Pinagadi_Meghana_0-1741859332792.png

Please help me with this error... pleaseeeee

Pinagadi_Meghana_0-1741859391665.png

please help me with this error... pleasee

please check my error... everything seems to be good.... please check it and tell me please