2025-07-06 11:50 PM - edited 2025-07-06 11:52 PM
Hello everyone,
I am currently working on a project with a STM32U545. There was a first prototype electronics + software that was working. I made a new hardware and I wanted to use the same code with just a few modification.
For this, I just copied the STM32CubeIDE project, modified the configurator with the integrated CubeMX, regenerated the code and compiled.
This is where I ran into problems:
I have this compilation error:
../Drivers/STM32U5xx_HAL_Driver/Inc/stm32u5xx_hal_uart_ex.h:231:36: error: unknown type name 'UART_HandleTypeDef'; did you mean 'RTC_HandleTypeDef'?
231 | HAL_StatusTypeDef HAL_RS485Ex_Init(UART_HandleTypeDef *huart, uint32_t Polarity, uint32_t AssertionTime,
| ^~~~~~~~~~~~~~~~~~
| RTC_HandleTypeDefSTM32Cube IDE version: 1.18.0
STM32CubeMX version: 6.14.0
When looking at the generated driver (file stm32u5xx_hal_uart.h), I noticed that the UART_HandleTypeDef was missing its name before the semicolon:
typedef struct __UART_HandleTypeDef
{
USART_TypeDef *Instance; /*!< UART registers base address */
UART_InitTypeDef Init; /*!< UART communication parameters */
UART_AdvFeatureInitTypeDef AdvancedInit; /*!< UART Advanced Features initialization parameters */
const uint8_t *pTxBuffPtr; /*!< Pointer to UART Tx transfer Buffer */
uint16_t TxXferSize; /*!< UART Tx Transfer size */
__IO uint16_t TxXferCount; /*!< UART Tx Transfer Counter */
uint8_t *pRxBuffPtr; /*!< Pointer to UART Rx transfer Buffer */
uint16_t RxXferSize; /*!< UART Rx Transfer size */
__IO uint16_t RxXferCount; /*!< UART Rx Transfer Counter */
uint16_t Mask; /*!< UART Rx RDR register mask */
uint32_t FifoMode; /*!< Specifies if the FIFO mode is being used.
This parameter can be a value of @ref UARTEx_FIFO_mode. */
uint16_t NbRxDataToProcess; /*!< Number of data to process during RX ISR execution */
uint16_t NbTxDataToProcess; /*!< Number of data to process during TX ISR execution */
__IO HAL_UART_RxTypeTypeDef ReceptionType; /*!< Type of ongoing reception */
__IO HAL_UART_RxEventTypeTypeDef RxEventType; /*!< Type of Rx Event */
void (*RxISR)(struct __UART_HandleTypeDef *huart); /*!< Function pointer on Rx IRQ handler */
void (*TxISR)(struct __UART_HandleTypeDef *huart); /*!< Function pointer on Tx IRQ handler */
#if defined(HAL_DMA_MODULE_ENABLED)
DMA_HandleTypeDef *hdmatx; /*!< UART Tx DMA Handle parameters */
DMA_HandleTypeDef *hdmarx; /*!< UART Rx DMA Handle parameters */
#endif /* HAL_DMA_MODULE_ENABLED */
HAL_LockTypeDef Lock; /*!< Locking object */
__IO HAL_UART_StateTypeDef gState; /*!< UART state information related to global Handle management
and also related to Tx operations. This parameter
can be a value of @ref HAL_UART_StateTypeDef */
__IO HAL_UART_StateTypeDef RxState; /*!< UART state information related to Rx operations. This
parameter can be a value of @ref HAL_UART_StateTypeDef */
__IO uint32_t ErrorCode; /*!< UART Error code */
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
void (* TxHalfCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Tx Half Complete Callback */
void (* TxCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Tx Complete Callback */
void (* RxHalfCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Rx Half Complete Callback */
void (* RxCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Rx Complete Callback */
void (* ErrorCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Error Callback */
void (* AbortCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Abort Complete Callback */
void (* AbortTransmitCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Abort Transmit Complete Callback */
void (* AbortReceiveCpltCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Abort Receive Complete Callback */
void (* RxFifoFullCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Rx Fifo Full Callback */
void (* TxFifoEmptyCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Tx Fifo Empty Callback */
void (* RxEventCallback)(struct __UART_HandleTypeDef *huart, uint16_t Pos); /*!< UART Reception Event Callback */
void (* MspInitCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Msp Init callback */
void (* MspDeInitCallback)(struct __UART_HandleTypeDef *huart); /*!< UART Msp DeInit callback */
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
}; // MISSING STRUCT NAME!I tried deleting the file and relaunch code generation but it did NOT solve the issue.
Do you have any lead?
Thanks a lot,
Arthur
Solved! Go to Solution.
2025-07-09 11:44 PM
Ok, si I updated to version 1.19.0 (CubeMX 6.15.0) and CubeMX does NOT regenerate HAL driver anymore.
I am pretty sure it was doing it before update. How can I force complete regeneration of HAL driver to make sure I am up to date?
Thank you
2025-07-10 12:41 AM - edited 2025-07-10 12:41 AM
I found a solution: After updating CubeIDE it seems there is a new MCU package for STM32U5 series (1.8.0). After updating I could make a clean regeneration of the HAL Driver and my inital problem (missing struct name in UART driver) is now solved.