CMake project bug in cubeMX6.14.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-31 1:09 AM
On a NUCLEO-H7S3L8 I've been testing the Projects/NUCLEO-H7S3L8/Applications/USBPD from STM32Cube_FW_H7RS_V1.2.0 with cubeMX6.14.0. I use the VScode extension, so I select the CMake toolchain. I select the "copy only necessary files" in code generation.
I noticed a different behaviour when I just copy the .ioc file from the example (and just select CMake) to when I use the "access to example selector" button of cubeMX. The .ioc file in the example does not specify the specific board: it has board=custom, while the one from the example selector has: BSP_IP_NAME=NUCLEO-H7S3L8 board=NUCLEO-H7S3L8. That is the only difference I see in the .ioc files.
The code generated from either of these does not operate correctly.
With example selector:
- BSP code is added in the folder and included in CMake files.
- The libraries are not referenced in CMake files. For example, all the *HAL_Driver/Src/* files are missing in set(STM32_Drivers_Src part of mx-generated.cmake. The same holds for all Middleware libraries.
- As a result, the project does not even build.
With copying the .ioc from the example:
- The BSP code is not added in the folder and it is not referenced in the CMake files.
- The libraries, however, are correctly referenced in the CMake files.
- As a result, the project builds, but because the BSP code for the board is missing, it does not work on the board.
There must be a bug somewhere in the code generation script, which does not produce the library references in the CMake files when BSP code is included. I haven't tried on anything other than CMake.
As a workaround, I just build both and then compare all the CMake related files and fix them.
- Labels:
-
Bug-report
-
STM32CubeMX
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-18 8:55 AM - edited 2025-04-18 8:55 AM
Hello @AEfth
Thank you for your contribution,
The issue is currently under investigation internally.
When you copy the .ioc from the example, you should copy .extSettings file as well that contain the BSP references, could you verify please?
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.