2022-08-11 01:04 AM
I was able to successfully install and launch CubeMX. However, I cannot download the packages. In my case I need the STM32CubeG0 firmware packages. When I download it manually and select "From Local" I get "Failed to create temporary directory". In ~/STMCube/Repository write permissions are granted.
If I start CubeMX as root, then everything works. But I don't want to start CubeMX always as root. How do I fix this problem?
2022-08-11 02:16 AM
Hi @MMett ,
Can you try modifying your default repository FW path to a directory that you are sure to have full write permissions.
Below a screenshot of the CubeMX option allowing you browsing your FW repository.
Then, re-start MX and perform a new FW installation trial.
Let me know your feedback.
Aymen.