cancel
Showing results for 
Search instead for 
Did you mean: 

CAN communication example running error (CAN_IT Module) in STM32-MAT/TARGET toolbox

Anjie Wang
Associate

Hello!

I am working with following softwares ,and I want to realize CAN communication via example in STM32Demos(D:\MATLAB\STM32-MAT\STM32\STM32demos\Test\CAN\F429I-DISC1\F4_CAN_LoopBackInterrupt)

matlab 2018b

STM32CubeMX 5.1.0

STM32-MAT/TARGET 5.1.0

Question​:

There is a error with CAN_IT module when running the example. As follows,

0690X000009Z6mwQAC.png

The attached are the Simulink model and the. IOC configuration file for STM32CubeMX.

1 REPLY 1
Anjie Wang
Associate

Please any help,thank you!