2023-02-03 3:14 AM
Hello,
Using
When generating with ETH interface, changing the Rx Mode from Polling Mode to Interrupt Mode do not change anything!
The ioc is changed, but none of the .c/.h files
2023-02-03 4:32 AM
Hello @ANauz.1 ,
Thanks for sharing this issue.
I added a couple of topics related to your post to give a broader audience of this post and increase its chance to be reviewed by our CubeMX experts.
Hello @Semer CHERNI,
Can you please take a closer look at this problem related to CubeMX.
Thanks
Imen
2023-02-03 6:06 AM
So, what should be modified to use the ETH in interruption mode?
2023-02-08 5:10 AM
Hello @ANauz.1 ,
Working with CubeMX 6.7.0 and F7 Firmware 1.17.0 and changing the Rx Mode from Polling Mode to Interrupt Mode in two different projects
And I found these changes in the project that uses "interrupt mode" as "Rx mode" in the following files:
Core\Inc\stm32f7xx_it.h
void ETH_IRQHandler(void);
Core\Src\stm32f7xx_hal_msp.c
/* ETH interrupt Init */
HAL_NVIC_SetPriority(ETH_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(ETH_IRQn);
Core\Src\stm32f7xx_it.c
/**
* @brief This function handles Ethernet global interrupt.
*/
void ETH_IRQHandler(void)
{
/* USER CODE BEGIN ETH_IRQn 0 */
/* USER CODE END ETH_IRQn 0 */
HAL_ETH_IRQHandler(&heth);
/* USER CODE BEGIN ETH_IRQn 1 */
/* USER CODE END ETH_IRQn 1 */
}
Hope this answered your question.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Regards,
Aymen
2023-02-14 1:32 AM
Hello,
I just test again and:
void ETH_IRQHandler(void);
Is present in Core\Inc\stm32f7xx_it.h in interrupt and polling mode
/**
* @brief This function handles Ethernet global interrupt.
*/
void ETH_IRQHandler(void)
{
/* USER CODE BEGIN ETH_IRQn 0 */
/* USER CODE END ETH_IRQn 0 */
HAL_ETH_IRQHandler(&heth);
/* USER CODE BEGIN ETH_IRQn 1 */
/* USER CODE END ETH_IRQn 1 */
}
Is present in Core\src\stm32f7xx_it.c in interrupt and polling mode
I have nothing about ETH It in Core\Src\stm32f7xx_hal_msp.c in interrupt and polling mode
So, in my configuration, (µC in TFBGA216, and Makefile), the generate project has no difference in interrupt nor polling mode on the ETH interface.
Regards,
Antoine
2023-02-15 12:41 AM
Hello @ANauz.1 ,
Could you please provide the project you are working on or your *.ioc file so I be able to investigate the issue.
Kind regards,
Aymen