Skip to main content
rbow021
Visitor II
October 8, 2019
Question

Bad Makefile generated by STM32CubeMX for STM32H745I-DISCO (failing to separate cores?)

  • October 8, 2019
  • 5 replies
  • 2011 views

Following a similar procedure described in this question, I tried choosing "Makefile" as my Toolchain/IDE. However, the generated Makefile has a couple of major problems.

Firstly, the C_SOURCES section had every file listed twice (specifically, it had a list of files, concatenated to itself.) This was easy enough to fix, giving the attached file. However, the next problem is far more difficult to deal with -- the result of running 'make' is as follows:

$ make
... <snip> ...
arm-none-eabi-gcc build/main.o build/stm32h7xx_it.o build/stm32h7xx_hal_msp.o build/main.o build/stm32h7xx_it.o build/stm32h7xx_hal_msp.o build/stm32h7xx_hal_cortex.o build/stm32h7xx_hal_tim.o build/stm32h7xx_hal_tim_ex.o build/stm32h7xx_hal_rcc.o build/stm32h7xx_hal_rcc_ex.o build/stm32h7xx_hal_flash.o build/stm32h7xx_hal_flash_ex.o build/stm32h7xx_hal_gpio.o build/stm32h7xx_hal_hsem.o build/stm32h7xx_hal_dma.o build/stm32h7xx_hal_dma_ex.o build/stm32h7xx_hal_mdma.o build/stm32h7xx_hal_pwr.o build/stm32h7xx_hal_pwr_ex.o build/stm32h7xx_hal.o build/stm32h7xx_hal_i2c.o build/stm32h7xx_hal_i2c_ex.o build/stm32h7xx_hal_exti.o build/stm32h7xx_hal_eth.o build/stm32h7xx_hal_eth_ex.o build/stm32h7xx_hal_fdcan.o build/stm32h7xx_ll_fmc.o build/stm32h7xx_hal_sdram.o build/stm32h7xx_hal_ltdc.o build/stm32h7xx_hal_ltdc_ex.o build/stm32h7xx_hal_dsi.o build/stm32h7xx_hal_qspi.o build/stm32h7xx_hal_sai.o build/stm32h7xx_hal_sai_ex.o build/stm32h7xx_ll_sdmmc.o build/stm32h7xx_hal_mmc.o build/stm32h7xx_hal_mmc_ex.o build/stm32h7xx_hal_uart.o build/stm32h7xx_hal_uart_ex.o build/stm32h7xx_hal_pcd.o build/stm32h7xx_hal_pcd_ex.o build/stm32h7xx_ll_usb.o build/system_stm32h7xx_dualcore_boot_cm4_cm7.o build/startup_stm32h745xx_CM7.o build/startup_stm32h745xx_CM4.o -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -specs=nano.specs -Tstm32h745xx_flash_CM4.ld  -lc -lm -lnosys  -Wl,-Map=build/stm32h7demo_CM4.map,--cref -Wl,--gc-sections -o build/stm32h7demo_CM4.elf
 
/usr/lib/gcc/arm-none-eabi/7.3.1/../../../arm-none-eabi/bin/ld: build/main.o: in function `main':
/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/../CM4/Src/main.c:122: multiple definition of `main'; build/main.o:/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/../CM4/Src/main.c:122: first defined here
/usr/lib/gcc/arm-none-eabi/7.3.1/../../../arm-none-eabi/bin/ld: build/main.o: in function `Error_Handler':
/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/../CM4/Src/main.c:727: multiple definition of `Error_Handler'; build/main.o:/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/../CM4/Src/main.c:727: first defined here
/usr/lib/gcc/arm-none-eabi/7.3.1/../../../arm-none-eabi/bin/ld: build/main.o:/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/../CM4/Src/main.c:67: multiple definition of `Rx_Buff'; build/main.o:/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/../CM4/Src/main.c:67: first defined here
... <snip> ...
/usr/lib/gcc/arm-none-eabi/7.3.1/../../../arm-none-eabi/bin/ld: build/startup_stm32h745xx_CM4.o:(.isr_vector+0x0): multiple definition of `g_pfnVectors'; build/startup_stm32h745xx_CM7.o:(.isr_vector+0x0): first defined here
/usr/lib/gcc/arm-none-eabi/7.3.1/../../../arm-none-eabi/bin/ld: build/startup_stm32h745xx_CM4.o: in function `WAKEUP_PIN_IRQHandler':
/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/startup_stm32h745xx_CM4.s:111: multiple definition of `Default_Handler'; build/startup_stm32h745xx_CM7.o:/home/rbowmaker/stm32h7demo/firmware/stm32h7demo/startup_stm32h745xx_CM7.s:111: first defined here
... <snip> ...

The first thing of note is that CM4/Src/main.c and CM7/Src/main.c both apparently get compiled to build/main.o, so one will be clobbering the other. And then, with the build/main.o being listed twice, "multiple definition" errors occur for every symbol. Secondly, *_CM7.o files are conflicting with *_CM4.o files.

I am only just dipping my toes into dual-core ARM processor for the first time, so I'm just guessing here, but aren't the CM4 and CM7 builds supposed to be compiled into separate ELF/hex files? Is there any chance STM32CubeMX can be modified to generate valid Makefiles soon?

This topic has been closed for replies.

5 replies

SLuka.1
Associate II
December 28, 2019

Hi guys! Is there any ​solution for stm32h745i-disco? I'm also trying to build project using makefile from cube, but... unsuccessful. Maybe someone have any example of makefile for dual-core processor? Any help wil be appreciated.

JHeye.793
Visitor II
January 24, 2020

Hi,

I wrote a small tool for my personal use case (STM32H755 Nucleo ZI-Q model) which takes as input a generated SW4STM32 project (tested with output from STM32Cube_FW_H7_V1.5.0) and generates a Makefile taking the relevant information from the .cproject file and the *.c files in the directory.

The tool is a little rough (for example, make clean may be necessary before building with make) and I only cared about my specific MCU for now, but the Makefile is able to correctly generate binaries for the CM7 and CM4.

Would the community be interested in something like that? I might extract it from my current project and publish it on my gitlab account.

Jens

Beni1
Associate II
February 8, 2020

Hi!

I think Makefile generation was never the main focus of ST for some reason. There used to be scripts around for Makefile generation from different type of projects.. (ex.: https://gist.github.com/roberthartung/164788137759fea98868)

It would be great if you could share it as dont want to sink too much effort in making one if the next version of cubemx will be supporting it anyway..

Thanks,

Beni

Dookei
Visitor II
September 6, 2022

Hi ,

3 years later and there is still no solution... I also would like to generate the makefile for this MCU family.

SLuka.1
Associate II
September 6, 2022

There is no problem to write it by yourself. I'm using only makefile projects in my work, also on STM32H745.​