cancel
Showing results for 
Search instead for 
Did you mean: 

After programming going to execute not happening. I normally keep the controller in boot mode and load the code either through serial port or USB depending on the controller. In this case it is 103C8 controller. I use STM CUBE Programmer.

Parmin Nayani
Associate III

I tick the "Run after programming" option. Normally this works fine. User code gets going after programming. I create projects using Cube MX. With latest Cube MX (Version 6.4.0) code, after programming control is not going to user code. I have to now change the BOOT selection jumper and press reset. Then only user code is being executed. I never faced this problem before with earlier version (I don't have the older version number, as I upgraded Cube MX). I took one of my earlier projects and changed the code to test this feature manually and it works fine. Soon after downloading the code control transfers to user code. Can someone point out why this is happening and what is the solution please? Thank you for your valuable time.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0