2020-11-25 04:29 PM
Shouldn't CubeMX 6.01 create the #defines that coorespond to newly added User Labels in an existing project ?
Of course it works if I add the User Labels as #defines manually.
If this is the expected design behavior, please let me know...
Thanks,
Heather
Solved! Go to Solution.
2020-12-07 06:14 AM
Hi @HGran.1 ,
Any feedback ? do you confirm that CubeMX 6.1.0 fix your issue?
Khouloud
2020-12-04 12:32 AM
Hello @HGran.1
Can you please check with the 6.1.0 CubeMX version if problem still exist or not ?
Thanks, Khouloud
2020-12-07 06:14 AM
Hi @HGran.1 ,
Any feedback ? do you confirm that CubeMX 6.1.0 fix your issue?
Khouloud
2021-02-15 11:09 AM
Hi there,
I had the same problem. The reason for me was pretty simple.
Since I am working on a dual core, I had to assign a "Pin Context" (M7 or M4).
After having assigned that, it worked as expected.
Here is a screenshot of the configuration
Hope it helps you too!
Johannes