cancel
Showing results for 
Search instead for 
Did you mean: 

USB Driver for power monitor.

SSmit.13
Senior

Hi

  I have the cube monitor plugged in , and running the cube monitor power application. I had it working on my old computer (Windows 10) , but had to install the USB driver of ST web site. Since moving to my new computer, I cant find the driver again. Anyone point me to where it will be? My new computer is WIndows 10 too, and installing the cube monitor power application doesnt install the driver

 

Many thanks

Scott

1 ACCEPTED SOLUTION

Accepted Solutions
PDEFO.1
ST Employee

Hi,

Hello, I suggest this driver which is available here: https://www.st.com/en/development-tools/stsw-link009.html

BR

Philippe

View solution in original post

2 REPLIES 2
PDEFO.1
ST Employee

Hi,

Hello, I suggest this driver which is available here: https://www.st.com/en/development-tools/stsw-link009.html

BR

Philippe

Please find hereafter the description and features of this driver

Description
This USB driver (STSW-LINK009) is for ST-LINK/V2, ST-LINK/V2-1, and STLINK-V3 boards and derivatives (STM8/STM32 Discovery kits, STM8/STM32 Evaluation boards, and STM32 Nucleo boards). It declares the USB interfaces possibly provided by the ST-LINK to the system: ST Debug, Virtual COM port, and ST Bridge interfaces.

Installing the driver before connecting the ST-LINK/V2 or ST-LINK/V2-1 devices is mandatory for a successful enumeration. Installing the driver before connecting STLINK-V3 devices is optional to customize the default names assigned by the system to Virtual COM ports.

All features
Digitally signed driver
WinUSB CoInstallers for x86 (32-bit) and amd64 (64-bit) versions of Windows® 10 and 11 (Not tested on Windows® 7 and 8)
ST-LINK USB interface descriptors (Debug, Bridge, Virtual COM port)