2022-01-11 07:06 AM
Sometimes you need to reset the device and I use quite often (even it is not professional) the CubeMX Programmer with SWD to reset the device.
A button to do this would be great?
2022-01-11 07:15 AM
Welcome, @Community member, to the community!
where would you like to have a button?
As a software button: it can already be found within the STM32CubeProgrammer on the left-hand side under the CPU item.
As a hardware button: you can add it to your design at any time: just connect it between NRST and GND. It is already present on NUCLEO, DISCOVERY or other ST boards.
Regards
/Peter
2022-01-11 07:36 AM
No I like a software button in the STM32CubeMonitor
so I can add a button with hardware reset to the dashboard or even trigger it by a variable or something else ..