2022-03-23 5:17 AM
Hi everyone.
I'm trying to secure STM32CubeMonitor Editor and UI as defined to Node-RED, but is not possible secure STM32CubeMonitor.
After define a user and password at settings.js (even only for STM32 CubeMonitor) the editor and UI breaks and are simply useless.
This is a critical issue nowadays, not been able to secure a webserver that can be exposed to remote access, to provide REST API's and so on...
Tested STM32CubeMonitor v1.3.0
In other hand, this features works perfectly on native Node-RED instances.
There is a known workaround to secure STM32CubeMonitor editor and UI with user-password login?
Solved! Go to Solution.
2022-10-31 9:46 AM
Hi @Andrea cavani
The release 1.5.0 is online. It should be possible now to secure the editor properly.
Please, let us know if it is ok with the new version.
Please note: In the default setting.js, the remote access is now disabled by default.
Best regards
Stephane