cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0B1 NRST not pinned?

XD
Associate III

Hi, 

Not sure if this is an issue or if I'm missing something.

Shouldn't the processors reset-pin be pinned by default even though it allows for alternative functions?

Maybe this is a non issue, but I feel like the reset pin is somewhat critical.

XD_0-1742131303016.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Pin 10 is tied to both PF2 and NRST. Not one or the other, but both. You can change the NRST functionality in the option bytes but by default it functions as a normal NRST pin.

If you configure PF2 as an output and set it low, the chip will reset (and be hard to connect to, so don't do it).

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

Pin 10 is tied to both PF2 and NRST. Not one or the other, but both. You can change the NRST functionality in the option bytes but by default it functions as a normal NRST pin.

If you configure PF2 as an output and set it low, the chip will reset (and be hard to connect to, so don't do it).

If you feel a post has answered your question, please click "Accept as Solution".