cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMonitor 1.10 on Windows does NOT start

kojima
Associate III

Dear staffs,

I'm going to use "STM32CubeMonitor" for several Nucleo boards, such as Nucleo144 of STM32H563.

But, when I try to invoke, following dialog appears and does not proceed.

Why ?

kojima_0-1742944219572.png

Thank you 

9 REPLIES 9
Richard.Chvr
ST Employee

Sounds strange, can you try on another port?

Need to edit settings.js file (in <YourDrive>\Users\<xxxxxx>\.STMicroelectronics\stm32cubemonitor)

change line :

/** the tcp port that the Node-RED web server is listening on */ uiPort: process.env.PORT || 1880,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
kojima
Associate III

Oh.. That's port for Node-RED...

My "setting.js" file includes that port setting description line.

can you try on another port?

Do you mean, change port number such as 1881 in stread of 1880 ?

 

kojima
Associate III

I tried several "188x"  but, same results...

Richard.Chvr
ST Employee

Ok , is this error happening at STM32CubeMonitor start or upon deploy ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Richard.Chvr
ST Employee

When you change to "188x" , was the reported error on that 188x port or still on 1880

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
kojima
Associate III

New errors represents each changed port number, not still on 1880.

Richard.Chvr
ST Employee

Looks like an application is using the 188x ports

Can you try on another rand 808x for exampl

You can also check port availability thank to

netstat -ano | find /i "<host_address:port_number>"

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
kojima
Associate III

Sorry for my delay response.

I tried ”netstat -ano" command. But, no reported line related to port 1880 etc.. was seen in the response.

I also tried on TCP port 8080 as you advised. But same result as bellow.

kojima_0-1743633971950.png

There is no doubt that something is happening.

But, that might not the what error report dialog says....

Pavel A.
Super User

There is no doubt that something is happening.

No doubt. Is any VPN or "security" software installed? especially Zoho/Manage Engine?