2022-10-12 6:56 PM
Another computer can ping the host successfully , but can't connect to Dashboard. My phone and ipad are the same.
What should I do?
Solved! Go to Solution.
2022-10-14 5:03 AM
Hello
There is no special configuration in the picture, we just use it to see the IP address.
Some point to check :
Best regards
Stephane
2022-10-12 7:03 PM
Is this address the host ip address or the router ip address?
2022-10-13 5:36 AM
Hello
It is the address of the host computer. (The computer running STM32CubeMonitor)
You can find more information in this video : https://youtu.be/jlCLrg-yxN8
Best regards
Stephane
2022-10-13 7:22 PM
Thank you.
I have watched this video many times before, and my understanding is that the host, mobile phone and ipad are in the same local area network. Even in the same local area network, other devices still cannot connect to the host address (ipv4), is there any configuration required for the router (but I can ping my computer with other computers, when I enter http://Ip address:1880/ , no dashboard found).:face_with_tears_of_joy:
Is there anything special about this configuration in the picture?
2022-10-14 5:03 AM
Hello
There is no special configuration in the picture, we just use it to see the IP address.
Some point to check :
Best regards
Stephane
2022-10-14 6:31 AM
Hello
Thank you for your help.
I don't where to find this setting file.
Best regards
Lh
2022-10-14 6:43 AM
It is in the general settings file. It is explained in this wiki :
https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:How_to_change_general_settings
Best regards
2022-10-14 6:46 AM
:beaming_face_with_smiling_eyes: Thank you.