cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the scale for my Chart?

OVeli.1
Associate II

Dear all,

is it possible to change the Y scale for Chart? In the information panel I can see group

[Home] Chartorder4

width"7"

height"5"

chartType"line"

curveType"linear"

duration"10"

ymin""

ymax""

, but in the Properties tab I can see only group, size, chart type, curve type, duration and name... Scale is missed.

1 ACCEPTED SOLUTION

Accepted Solutions
Landry
Senior

Dear @OVeli.1​ ,

These ymin & ymax attributes are only available for Bar chart type :

" Y-Axis : Allows to define the Y axis lower and upper bounds for a bar chart. If the min and/or max value(s) is (are) not set, the bar chart will autoscale to any values received (with the 0 value centered in the middle of the graph). "

If you select the chart type Bar chart, you will see attributes Y-Axis.

View solution in original post

1 REPLY 1
Landry
Senior

Dear @OVeli.1​ ,

These ymin & ymax attributes are only available for Bar chart type :

" Y-Axis : Allows to define the Y axis lower and upper bounds for a bar chart. If the min and/or max value(s) is (are) not set, the bar chart will autoscale to any values received (with the 0 value centered in the middle of the graph). "

If you select the chart type Bar chart, you will see attributes Y-Axis.