cancel
Showing results for 
Search instead for 
Did you mean: 

Dinamically change chart Y axis min and max

Myzhar
Associate III

Hi,

I would like to set the minimum and maximum values of a dashboard chart using custom values calculated with a processing node.

I tried "single value" and "change" nodes, but without success.

I attached my current flow...

Thank you

Walter

12 REPLIES 12
A.D.
Senior

I'm also supporting this idea! Manually setting the limits of the chart would be very helpful in quite a few cases. Are there any current plans to include this functionality?

Don't get me wrong: Autoscaling is helpful very often. But sometimes it is not...

@Thierry 
Any news on the state of implementation of this?
I noticed that the chart's help shows that there's a property "Y-Axis" where one can manually set the limits but I cannot see this property in the actual chart settings.

Hello @DMeie.2 .
"Y-Axis" property is only available for Bar Chart type.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.