cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.13.0 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.13.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.13.0?
    • Added the support for new microcontrollers in the STM32U5 series
    • Added the support for new microcontrollers in the STM32WBA series
    • Added the support for two new boards related to the STM32U5 series: STM32U5G9J-DK1 and STM32U5G9J-DK2
    • Added the support for one new board related to the STM32L4+ series: STEVAL-SMARTAG2
    • Added the user authentication interface to permit package download
    • Updated to Eclipse® 2023-03
    • Updated to GCC 11 support by default
    • Added CMake project support
  • Updated debug:
    • Changed values highlighted in yellow in the SFRs view
    • Debug authentication for STM32H5 products
    • Support for programming using multiple external loaders with OpenOCD
  • Updated for microprocessors:
    • Support for the latest release 5.0.0 of OpenSTLinux
    • Addition of the TCP console for semihosting output
  • Main fixed issues
    • 109036 [UC5-REGENERATE][CubeIDE][Examples]Build failed when changing some configurations of LoRaWAN_End_Node example
    • 131635 Add option to highlight when a live variable changes its value
    • 143369 STM32CubeMX Linker script generation problem
  • Known issues fixed and problems and limitations
    • Please refer to the wiki.
  • Where do I obtain STM32CubeIDE 1.13.0?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0 REPLIES 0