STM32CubeIDE 1.13.0 was released today on st.com as well as an in-tool update patch.
- What is new in 1.13.0?
- Added the support for new microcontrollers in the STM32U5 series
- Added the support for new microcontrollers in the STM32WBA series
- Added the support for two new boards related to the STM32U5 series: STM32U5G9J-DK1 and STM32U5G9J-DK2
- Added the support for one new board related to the STM32L4+ series: STEVAL-SMARTAG2
- Added the user authentication interface to permit package download
- Updated to Eclipse® 2023-03
- Updated to GCC 11 support by default
- Added CMake project support
- Updated debug:
- Changed values highlighted in yellow in the SFRs view
- Debug authentication for STM32H5 products
- Support for programming using multiple external loaders with OpenOCD
- Updated for microprocessors:
- Support for the latest release 5.0.0 of OpenSTLinux
- Addition of the TCP console for semihosting output
- Main fixed issues
- 109036 [UC5-REGENERATE][CubeIDE][Examples]Build failed when changing some configurations of LoRaWAN_End_Node example
- 131635 Add option to highlight when a live variable changes its value
- 143369 STM32CubeMX Linker script generation problem
- Known issues fixed and problems and limitations
- Please refer to the wiki.
- Where do I obtain STM32CubeIDE 1.13.0?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.