2022-01-16 11:45 PM
Good afternoon.I tried to create a demo project (STM32MP157C-DK2\Demonstrations\Al_Character_Recognition) for the STM32MP157D_DK1 board. When assembling, I had a problem.(Gluk_test_1) How to include the library in the project correctly? Sincerely, Alexander.
2022-02-09 02:08 AM
Dear @Vlaty.1 ,
I think the original question was answered (How to include the library in the project correctly?) and this is a new issue.
Could you please open a new thread for this new issue?
Thank you ..
2022-02-09 02:32 AM
No. I got around this problem. The problem with the unstable operation of the STM32MP157D-DK board. The operation of the time output program on the console leads to a restart of the system after an hour (Openstlinux)
2022-02-09 02:44 AM
For the efficiency and to have answers from the community members, It's better for you to open another thread with the right title.. Otherwise, I'm afraid, you have a risk to not get an answer ..
2022-02-09 02:49 AM
OK