2024-07-30 04:22 PM
I've installed the latest Cube, 1.16.0, and configured a DAC and PWM. The code generated fine but I wanted to add FreeRTOS. So I added it under the Middleware dropdown and it does appear to install. However, when I generate code I do not get any FreeRTOS support.
Previously, in 1.14.0, I would see FreeRTOS in the Middlewares directory. Now I don't even have a Middlewares directly and there is not FreeRTOS support in my generated code.
Any ideas what is going on here?
thanks,
Jeff