2025-02-24 08:13 AM - last edited on 2025-02-24 08:40 AM by Andrew Neil
Moved from the MPUs section - STM32H7 is an MCU.
I have a software example for the STM32H743 provided by STMicroelectronics and I want to add the IOC corresponding to my micro, which is the STM32H753.
It does not have the IOC of the STM32H743.
I use Cube IDE V 1.17; is it possible?, or at least add the ioc of the STM32H743 thanks
2025-02-24 08:37 AM - edited 2025-02-24 08:38 AM
@yogui_ricardo wrote:I have a software example for the STM32H743 provided by STMicroelectronics
Which example, exactly?
Yes, it is true that not all examples have .ioc files - see: