cancel
Showing results for 
Search instead for 
Did you mean: 

Why do I get these errors when doing a release build but no errors when doing a debug build? A clean before building has no effect..

JPonk.1
Associate II

Build environment:

STM32CubeIDE

Version: 1.6.1

Build: 9958_20210326_1446 (UTC)

Linux Mint 19.2

arm-none-eabi-g++ (15:6.3.1+svn253039-1build1) 6.3.1 20170620

-----------------------------------------------------------------------------------------------------------

21:46:25 **** Incremental Build of configuration Release for project I2S-RXTX-F7 ****

make -j4 all

arm-none-eabi-g++ -o "I2S-RXTX-F7.elf" @"objects.list" -larm_cortexM7lfdp_math -mcpu=cortex-m7 -T"/home/jponko/opt/STM32CubeIDE/workspace/I2S-RXTX-F7/STM32F767ZITX_FLASH.ld" -Wl,-Map="I2S-RXTX-F7.map" -Wl,--gc-sections -static -Wl,--start-group -larm_cortexM7lfdp_math -Wl,--end-group -L"/home/jponko/opt/STM32CubeIDE

/workspace/I2S-RXTX-F7/lib" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb

-Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group

/opt/st/stm32cubeide_1.6.1/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.linux64_1.5.0.202011040924/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld: Core/Startup/startup_stm32f767zitx.o: in function `LoopFillZerobss':

(.text.Reset_Handler+0x32): undefined reference to `main'

collect2: error: ld returned 1 exit status

make: *** [makefile:80: I2S-RXTX-F7.elf] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

21:46:26 Build Failed. 3 errors, 0 warnings. (took 524ms)

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TheaArt
Associate III

Have the same problem here.

Debug compiles and links without errors, release does not.

I didn't change anything in the build configurations. But i looks as Release doesnt clean end compile my my own code. So functions called in main.c are not definded in object files (which are still there from Debug build since they are not cleaned in release build)

See attached files for clean and build loggings.

TheaArt
Associate III

Since I could only attach one file, here comes the debug build:

I'm not familiar to eclipse, so I dont want to change something I do not understand well. But there seemsto be something missing in the release build configuration.

Thank you.

So now I can answer for myself. Maybe someone could help this.

In my case all my code was in an extra folder. And, however, this folder was excluded from build in release configuration.

So solution was: switch to release configuration, then right click this directory, select properties (alternat. press ALT+Enter when folder is selected), select C/C++ Build in the tree view uncheck exclude from build checkbox.

S.Ma
Principal

IAR for example does not have dual debug and releaas as it is very easy to change the compile option which is mostly modified and debugged. It keeps the mind focused on the code rather than the toolchain split workspace....